Configure Controller Onboard I/O

The procedure to define the local I/Os of the PDMM or PCMM is very similar to the one for I/O slices. Note that the Onboard digital I/O is limited to a 1kHz update rate.

EtherCAT update rate Onboard digital I/O update rate
500Hz 500Hz
1kHz 1kHz
2kHz 1kHz
4kHz 1kHz

For more details, refer to Map Input and Output to Variables

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™